1. STM32CUBE.AI enabled OpenMV firmware
This tutorial will walk you through the process of integrating your own neural network into the OpenMV environment.
The OpenMV open-source project provides the source code for compiling the OpenMV H7 firmware with STM32Cube.AI enabled.
The process for using Cube.AI with OpenMV is described in the following figure.
- Train your neural network using you favorite deep learning framework.
- Convert your trained network to optimized C code using ST Cube.AI tool
- Download the OpenMV firmware source code, and
- Add the generated files to the firmware source code
- Compile with GCC toolchain
- Flash the board using OpenMV IDE
- Program the board with microPython and perform inference
1.1. Prerequisites
To follow this article it is assumed that a Linux environment is used (tested with Ubuntu 18.04).
All the command starting with this syntax should be executes in a Linux console:
<mycommand>
1.2. Requirements
1.2.1. Check that your environment is up to date
sudo apt update sudo apt upgrade sudo apt install git zip make build-essential tree
1.2.2. Create your workspace directory
mkdir $HOME/openmv_workspace
1.2.3. Install the stm32ai command line to generate the optimized code
- Download the latest version of the X-CUBE-AI expansion pack from ST website into your openmv_workspace directory
- Extract the archive
cd $HOME/openmv_workspace chmod 644 en.x-cube-ai-v5-0-0.zip unzip en.x-cube-ai-v5-0-0.zip mv STMicroelectronics.X-CUBE-AI.5.0.0.pack STMicroelectronics.X-CUBE-AI.5.0.0.zip unzip STMicroelectronics.X-CUBE-AI.5.0.0.zip -d X-CUBE-AI.5.0.0
- Add the stm32ai command line to your PATH.
export PATH=$HOME/openmv_workspace/X-CUBE-AI.5.0.0/Utilities/linux:$PATH
You can verify that the stm32ai command line is properly installed:
stm32ai --version stm32ai - Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0)
1.2.4. Install the GNU Arm toolchain version 7-2018-q3 to compile the firmware
sudo apt remove gcc-arm-none-eabi sudo apt autoremove sudo -E add-apt-repository ppa:team-gcc-arm-embedded/ppa sudo apt update sudo -E apt install gcc-arm-embedded
You can verify that the GNU Arm Toolchain is properly installed:
arm-none-eabi-gcc --version arm-none-eabi-gcc (GNU Tools for Arm Embedded Processors 7-2018-q3-update) 7.3.1 20180622 (release) [ARM/embedded-7-branch revision 261907] Copyright (C) 2017 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
1.2.5. Install the OpenMV IDE
Download OpenMV IDE from OpenMV website.
OpenMV IDE will be used to develop microPython scripts and to flash the board.
1.3. Step 1 - Download and prepare the OpenMV project
In this section we will clone the OpenMV project, checkout a known working version and create a branch.
Then we will initialize the git submodules. This will clone OpenMV dependencies, such as microPython.
1.3.1. Clone the OpenMV project
cd $HOME/openmv_workspace git clone https://github.com/openmv/openmv.git
1.3.2. Checkout a known working version
cd openmv git checkout b4bad33 -b cubeai
1.3.3. Download micropython submodule and necessary dependencies
- Download micropython submodule
git submodule update --init
- Download only necessary dependencies (lib/berkeley-db-1.xx and lib/stm32lib)
cd src/micropython git submodule update --init lib/berkeley-db-1.xx lib/stm32lib
1.4. Step 2 - Add the Cube.AI library to OpenMV
Now that the OpenMV firmware is downloaded, we need to copy over the Cube.AI runtime library and header files into the OpenMV project.
cd $HOME/openmv_workspace/openmv/src/stm32cubeai mkdir -p AI/{Inc,Lib} mkdir data
Then copy the files from Cube.AI to the AI directory:
cp $HOME/openmv_workspace/X-CUBE-AI.5.0.0/Middlewares/ST/AI/Inc/* AI/Inc/ cp $HOME/openmv_workspace/X-CUBE-AI.5.0.0/Middlewares/ST/AI/Lib/ABI2.1/STM32H7/NetworkRuntime*_CM7_IAR.a AI/Lib/NetworkRuntime_CM7_GCC.a
After this operation, the AI directory should look like this
AI/ ├── Inc │ ├── ai_common_config.h │ ├── ai_datatypes_defines.h │ ├── ai_datatypes_format.h │ ├── ai_datatypes_internal.h │ ├── ai_log.h │ ├── ai_math_helpers.h │ ├── ai_network_inspector.h │ ├── ai_platform.h │ ├── ... ├── Lib │ └── NetworkRuntime_CM7_GCC.a └── LICENSE
1.5. Step 3 - Generate the code for a NN model
In this section, we will train a convolutional neural network to recognize hand-written digits.
We will then generate a STM32 optimized C code for this network thanks to STM32Cube.AI.
These files will be added to OpenMV firmware source code.
1.5.1. Train a convolutional neural network
The convolutional neural network for digit classification (MNIST) from Keras will be use as an example. If you want to train the network, you need to have Keras installed.
To train the network and save the model to the disk, run the following commands:
cd $HOME/openmv_workspace/openmv/src/stm32cubeai/example python3 mnist_cnn.py
1.5.2. STM32 optimized code generation
To Generate the STM32 optimized code, use the stm32ai command line tool as follow:
cd $HOME/openmv_workspace/openmv/src/stm32cubeai stm32ai generate -m example/mnist_cnn.h5 -o data/
The following files will be generated in $HOME/openmv_workspace/openmv/src/stm32cubeai/data:
* network.h * network.c * network_data.h * network_data.c
1.5.3. Preprocessing
If you need to do some special preprocessing before running the inference, you should modify the function ai_transform_input
located into src/stm32cubeai/nn_st.c
. By default, the code does the following:
- Simple resizing (subsampling)
- Conversion from unsigned char to float
- Scaling pixels from [0,255] to [0, 1.0]
The provided example might just work out of the box, but you may want to take a look at this function.
1.6. Step 4 - Compile
- Edit omv/boards/OPENMV4/omv_boardconfig.h line 76 and set OMV_HEAP_SIZE to 230K. This will lower the heap section in RAM allowing more space for our neural network activation buffers.
- Execute the following command to compile:
cd $HOME/openmv_workspace/openmv/src/ make clean make CUBEAI=1
1.7. Step 5 - Flash the firmware
- Plug the OpenMV camera to the computer using a micro-USB to USB cable.
- Open OpenMV IDE
- From the toolbar select Tools > Run Bootloader
- Select the firmware file (It is located in openmv/src/build/bin/firmware.bin) and follow the instructions
- Once this is done, you can click the Connect button located at the bottom left of the IDE window
1.8. Step 6 - Program with microPython
- Open OpenMV IDE, and click the Connect button located at the bottom left of the IDE window
- Create a new microPython script File > New File
- You can start from this example script running the MNIST neural network we have embedded in the firmware
'''
Copyright (c) 2019 STMicroelectronics
This work is licensed under the MIT license
'''
# STM32 CUBE.AI on OpenMV MNIST Example
import sensor, image, time, nn_st
sensor.reset() # Reset and initialize the sensor.
sensor.set_contrast(3)
sensor.set_brightness(0)
sensor.set_auto_gain(True)
sensor.set_auto_exposure(True)
sensor.set_pixformat(sensor.GRAYSCALE) # Set pixel format to Grayscale
sensor.set_framesize(sensor.QQQVGA) # Set frame size to 80x60
sensor.skip_frames(time = 2000) # Wait for settings take effect.
clock = time.clock() # Create a clock object to track the FPS.
# [CUBE.AI] Initialize the network
net = nn_st.loadnnst('network')
nn_input_sz = 28 # The NN input is 28x28
while(True):
clock.tick() # Update the FPS clock.
img = sensor.snapshot() # Take a picture and return the image.
# Crop in the middle (avoids vignetting)
img.crop((img.width()//2-nn_input_sz//2,
img.height()//2-nn_input_sz//2,
nn_input_sz,
nn_input_sz))
# Binarize the image
img.midpoint(2, bias=0.5, threshold=True, offset=5, invert=True)
# [CUBE.AI] Run the inference
out = net.predict(img)
print('Network argmax output: {}'.format( out.index(max(out)) ))
img.draw_string(0, 0, str(out.index(max(out))))
print('FPS {}'.format(clock.fps())) # Note: OpenMV Cam runs about half as fast when connected
Take a white sheet of paper and draw numbers with a black pen, point the camera towards the paper. The code should yield the following output:
2. Documentation of microPython CUBE.AI wrapper
This section provide information about the 2 microPhyton functions added the the OpenMV microPython framework in order to be able to initialize and run CUBE.AI optimized neural network inference.
2.1. loadnnst
nn_st.loadnnst(network_name)
Initialize the network named network_name.
Arguments:
- network_name : String, usually 'network'
Returns:
- A network object, used to make predictions
Example:
import nn_st
net = nn_set.loadnnst('network')
2.2. predict
out = net.predict(img)
Runs a network prediction with img as input.
Arguments:
- img : Image object, from the image module of nn_st. Usually taken from sensor.snapshot()
Returns:
- Network predictions as an python list
Example:
import sensor, image, nn_st
# Init the sensor
sensor.reset()
sensor.set_pixformat(sensor.RGB565)
sensor.set_framesize(sensor.QVGA)
# Init the network
net = nn_st.loadnnst('network')
# Capture a frame
img = sensor.snapshot()
# Do the prediction
output = net.predict(img)