New pages

New pages
Hide bots | Show redirects
  • 14:43, 31 October 2024STM32 KeygenTool (hist | edit) ‎[5,583 bytes] ‎Registered User (Created page with "KeygenTool for N6 : to be filled Category:STM3_Signing_and_Keygen_tools") Tag: 2017 source edit originally created as "Page:STM32 KeygenTool"
  • 14:39, 31 October 2024STM32 SigningTool (hist | edit) ‎[13,163 bytes] ‎Registered User (Created page with "Signingtool for N6 : to bedf illed Category:STM3_Signing_and_Keygen_tools") Tag: 2017 source edit originally created as "Page:STM32 SigningTool"
  • 10:57, 28 October 2024STM32WB0 2.4 GHz Radio and driver (hist | edit) ‎[21,286 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE: STM32WB0 2.4 GHz Radio and driver}} This document provides general information about the STM32WB0 series 2.4 GHz Radio and related HAL driver. The STM32WB0 series 2.4 GHz Radio HAL driver provides the capability to send and receive packets without using the Bluetooth link layer. == Introduction== The STM32WB0 series 2.4 GHz radio HAL driver interface controls the 2.4 GHz radio and it interacts with the Radio timer, which runs on the slow 32 kHz clock,...") Tag: 2017 source edit
  • 15:18, 22 October 2024STM32WB0 Bluetooth® LE PAwR/ESL features and applications (hist | edit) ‎[15,758 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE:STM32WB0 Bluetooth® LE PAwR/ESL features and applications}} This document provides general information about the Bluetooth LE Periodica Advertising with Response (PAwR) feature. It then introduces the STM32WB0 application examples built on top of the PAwR features. Further it provides the reference to dedicated PAwR/ESL applications examples supporting a real ESL PCB and available on STM32 hotspot. == Introduction== The legacy Bluetooth LE adverting pa...") Tag: 2017 source edit
  • 10:29, 22 October 2024How to configure and run I3C to communicate with sensors using HAL I3C Ctrl MultipleTransfer IT () (hist | edit) ‎[10,859 bytes] ‎Registered User (Created page with "This article provides a description of the I3C transmission/reception using an STM32H5xx Nucleo and the sensor LSM6DSO present on X-NUCLEO-IKS01A3. The goal of this example is to demonstrate a simple communication with the sensor LSM6DSO present on X-NUCLEO-IKS01A3 using '''HAL_I3C_Ctrl_MultipleTransfer_IT ()''' . The'''HAL_I3C_Ctrl_MultipleTransfer_IT()''' function allow the I3C Controller to send and receive an amount of data to or from the LSM6DSO Temperature, Gyrosc...") Tag: 2017 source edit
  • 09:55, 17 October 2024I3C private communication between STM32H5xx Nucleo and X-NUCLEO-IKS01A3 (hist | edit) ‎[0 bytes] ‎Registered User (Created page with "This article provides a description of the I<sup>3</sup>C transmission/reception using an STM32H5xx Nucleo and the sensor LSM6DSO present on X-NUCLEO-IKS01A3.") Tag: 2017 source edit
  • 13:27, 8 October 2024STM32CubeWB0 Bluetooth® LE MCU Package (hist | edit) ‎[14,091 bytes] ‎Registered User (New Doc for STM32CubeWB0) Tag: 2017 source edit
  • 14:51, 1 October 2024STM32WB0 Bluetooth® LE Stack Modularity and Integration (hist | edit) ‎[36,822 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE:STM32WB0 Bluetooth® LE Stack Modularity and Integration}} == '''Introduction''' == This wiki describes to an application developer the STM32WB0 series Bluetooth<sup>®</sup> LE stack library modularity feature and how to to integrate the Bluetooth<sup>®</sup> LE stack library on a user application<br> <br> {|style="margin-left: auto; margin-right: auto;" |- ! Acronym definitions |- | {| |- ! Acronym !! Definition |- | ACI || Application Controller Inter...") Tag: 2017 source edit
  • 08:09, 30 September 2024How to build a STM32WB0 Bluetooth® Low Energy project (hist | edit) ‎[8,440 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE: How to build a STM32WB0 Bluetooth<sup>®</sup> Low Energy project}} ==Presentation== This page describes how to build easily and install STM32WB0 Bluetooth® Low Energy example applications.<br> Project examples can be found on '''STM32CubeWBA MCU Package'''<ref name="STM32CubeWBA-Package">[https://www.st.com/en/embedded-software/stm32cubewba.html STM32CubeWBA MCU Package]</ref>, and are available for different platforms. {|style="margin-left: auto; margi...") Tag: 2017 source edit
  • 15:07, 26 September 2024STM32WB0 Bluetooth® Low Energy AOA feature (hist | edit) ‎[21,197 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE:STM32WB0 Bluetooth® Low Energy AOA feature}} The STM32WB09, STM32WB05 MCUs support the Bluetooth LE Direction Finding angle of arrival (AoA) and angle of departure (AoD) feature. This document provides the key concepts related to the Bluetooth LE Direction Finding and some information about how these featurec could be supported in the context of STM32WB09, STM32WB05 MCUs. == Introduction == Bluetooth Core Specification v5.1 introduced Direction findin...") Tag: 2017 source edit
  • 14:39, 26 September 2024STM32WB0 Bluetooth® LE network coprocessor (NCP) framework (hist | edit) ‎[29,604 bytes] ‎Registered User (Added page for STM32WB0 NCP) Tag: 2017 source edit
  • 13:57, 25 September 2024Category:STM32WB0 SW Package and Tools (hist | edit) ‎[195 bytes] ‎Registered User (Created page with "In this category you can find various project which can help you 40 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") originally created as "STM32WB0 SW Package and Tools"
  • 13:57, 25 September 2024Category:STM32WB0 Devices Features (hist | edit) ‎[195 bytes] ‎Registered User (Created page with "In this category you can find various project which can help you 35 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") originally created as "STM32WB0 Devices Features"
  • 13:56, 25 September 2024Category:STM32WB0 Bluetooth LE Features (hist | edit) ‎[195 bytes] ‎Registered User (Created page with "In this category you can find various project which can help you 30 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") originally created as "STM32WB0 Bluetooth LE Features"
  • 13:54, 25 September 2024Category:STM32WB0 Applications and Profiles (hist | edit) ‎[195 bytes] ‎Registered User (Created page with "In this category you can find various project which can help you 20 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") originally created as "Applications and Profiles"
  • 13:28, 16 September 2024Monitoring power supply with STM32 peripherals (hist | edit) ‎[49,928 bytes] ‎Registered User (Created page with "{{DISPLAYTITLE:Monitoring power supply with STM32 peripherals}} ==Introduction== The quality of the power supply is crucial for the reliability of electronic applications. The purpose of this article is to propose solutions to detect in real-time a degradation in the quality of the power supply or a disturbance that could alter the proper functioning of the application or it reliability. These solutions are based on STM32 embedded peripherals, thus avoiding the additio...") Tag: 2017 source edit