1. Wi-Fi Alliance
1.1. Presentation
The Wi-Fi Alliance is a global non-profit organization that promotes and certifies wireless networking technologies based on the IEEE 802.11 standards. Its mission is to enhance and promote the interoperability, security, and reliability of Wi-Fi products and services. T
Wi-Fi Alliance is responsible for developing and maintaining Wi-Fi standards, conducting certification programs, and promoting the adoption of Wi-Fi technology worldwide.
1.2. Eligibility to Certification
Only Wi-Fi Alliance Members can certify their products. There are multiple Level of membership.
- Example.jpg
Caption1
- Example.jpg
Caption2
Source: https://www.wi-fi.org/membership How to apply : https://www.wi-fi.org/membership-application
1.3. Why certify my product?
It is not mandatory to certify your product but WFA certification ensures that your product meets industry standards for performance, security and reliability, which means that it will provide a consistent and stable wireless connection.
1.4. Wi-Fi Certification Programs
The Wi-Fi Alliance offers several certification programs to ensure that Wi-Fi products meet industry standards for performance, reliability, and security. Here are some of the most common certification programs:
Wi-Fi CERTIFIED 4,5,6: This certification programs ensure that Wi-Fi products meet the Wi-Fi4 standards for high-speed, low-latency wireless connectivity.
Wi-Fi CERTIFIED WPA2, WPA3,PMF: This certification programs ensure that Wi-Fi products meet industry standards for improved security and privacy.
To have a complete view of all Certification programs , please refer to WFA Certification Programs
1.5. Certification Paths
Wi-Fi Alliance has developed 3 different paths to certify a product. It depends on the maturity of the device, if it has already been certified.
- Example.jpg
Caption1
- Example.jpg
Caption2
1.5.1. Flex Tack
FlexTrack path is designed for : - New products built from the ground-up. - Products that have been modified ( any modification related to Chipset, RF Architecture, Driver or Firmware ) - Products that have never been certified.
It allows more flexibility in WI-Fi customization. Flex Track complete full certification program with full test environment. Test will be completed at an Authorized Test Laboratory (ATL). Flex Track Cost, per product $5,000 license fee + ATL testing fees
To start Certification process: https://www.cert.wi-fi.org/#/application
1.5.2. QuickTrack
Quicktrack is designed for products based on an already certified solution.
Some targeted changes are allowed on the Wi-Fi solution: - Operating System - Antenna - RF component - Physical Interface
Testing can be done at an ATL lab or Memnber testing site.
Certify a new product using the QuickTrack certification path costs, per product $7,500 program license fee + ATL testing fees, if applicable.
1.5.3. Derivative path
Derivative path is designed for products that are excatly the same as the original. No changes are allowed on the Wi-Fi.
There is no need to perfom additional testig.
Certify a derivative product (based on your own company's Wi-Fi CERTIFIED product) costs $600 certification fee per derivative product.