STM32WBA Connection Subrating feature

Revision as of 16:00, 22 March 2024 by Registered User (→‎On-board buttons configuration)

1. Connection Subrating feature

It can sometimes be necessary for a device to use a low duty cycle connection for some use cases but be able to switch up to a high duty cycle when required to support other use cases.

Link Layer procedures that use "instants" such as the connection update procedure generally involve connection property changes that if not executed successfully by both devices can result in loss of connection.
To start the connection update procedure, the Host must send the controller a LE Connection Update command. The controller must respond by initiating the link layer Connection Update procedure, sending a LL_CONNECTION_UPDATE_IND PDU to the Peripheral with the Instant field specifying a connection event which is at least six events in the future at which point the connection parameter changes must be applied by both the Peripheral and Central.

Bluetooth® Connection update
Connectivity connection-update.png


Use cases which are expected to benefit from subrated connections include Bluetooth LE Audio products such as hearing aids and monitoring systems which use sensors.
An audio device like a hearing aid can maintain a subrated connection to a smartphone, making the connection available for immediate use when it becomes necessary to handle audio communication.
Subrating saves power but also allows the connected isochronous stream to be established very quickly.
Using subrated connections, a sensor can efficiently maintain a persistent, low duty cycle subrated connection to another device which collects sensor data.
When required it can then switch the connection up to a high duty cycle quickly so that accumulated sensor data can be uploaded over a higher bandwidth connection.

Bluetooth LE connections offer a highly flexible way to adapt to dynamic changes of requirements in terms of data throughput and power.
A high duty cycle connection achieves higher data throughput on the expense of increased power consumption, while a low duty cycle connection saves power on the expense of data throughput.

1.1. Connection subrating capabilities and benefits

The LE Enhanced Connection Update change introduces the concept of subrated connections.
A subrated connection achieves a power saving low duty cycle in a different way to non-subrated connections and is able to switch up to a high duty cycle more quickly.
Subrated connections are also able to handle variable packet rates or bursty traffic in an efficient way.
The ability to switch quickly from a low duty cycle connection to a high duty cycle connection when required and in a short time, will provide an improved user experience for some important product types and is the main benefit of the new subrated connections feature.

1.2. Connection subrating

1.2.1. Basic Principles

1.2.2. Subrate base events

1.3. how to implement on STM32WBA applications

Feature available in "full Link Layer" (use of "full ble stack") for STM32WBA.

1.3.1. Peripheral and Central

It is necessary to set connection subrating feature.

hci_le_set_host_feature

Description

This command is used by the Host to set or clear a bit controlled by the Host in the Link Layer FeatureSet stored in the Controller.
Syntax
tBleStatus hci_le_set_host_feature( uint8_t Bit_Number, uint8_t Bit_Value );
Parameters
[in] Bit_Number
Type: uint8_t
Description: Bit position in the FeatureSet. Is equal to 0x26 to set connection subrating feature.
[in] Bit_Value
Type: uint8_t
Description: Bit in the FeatureSet set/reset.
Return value
[out] command status
Type: uint8_t

1.3.2. Peripheral or Central

After LE link establishment, the central requires subrating.

hci_le_subrate_request

Description

This command is used by a Central or a Peripheral to request a change to the subrating factor and/or other parameters applied to an existing connection using the Connection Subrate Update procedure.
Syntax
tBleStatus hci_le_subrate_request( uint16_t Connection_Handle, uint16_t Subrate_Min, uint16_t Subrate_Max, 
uint16_t Max_Latency, uint16_t Continuation_Number, uint16_t Supervision_Timeout );
Parameters
[in] Connection_Handle
Type: uint16_t
Description: Connection handle for which the command applies.
[in] Subrate_Min
Type: uint16_t
Description: Minimum subrate factor.
[in] Subrate_Max
Type: uint16_t
Description: Maximum subrate factor.
[in] Max_Latency
Type: uint16_t
Description: Maximum Peripheral latency allowed in requests by a Peripheral, in units of subrated connection intervals.
[in] Continuation_Number
Type: uint16_t
Description: Minimum number of underlying connection events to remain active after a packet containing a Link Layer PDU with a non-zero Length field is sent or received in requests by a Peripheral.
[in] Supervision_Timeout
Type: uint16_t
Description: Supervision timeout for the LE Link. It shall be a multiple of 10 ms and larger than (1 + connPeripheralLatency) * connInterval * 2. Time = N * 10 ms.
Return value
[out] command status
Type: uint8_t

2. Example of Connection subrating feature on STM32WBA

2.1. Advertising data

At startup, Connection subrating Server application starts Advertising.
Data advertised are composed as follows:

Connection subrating Server Advertising packet
Description Length AD Type Value
Device Name 8 0x09 CS_XX (XX: last byte of BD address)
Manufacturer Data 15 0xFF See table below
Flags 2 0x01 0x06
(GeneralDiscoverable, BrEdrNotSupported)



Manufacturer data are encoded following STMicroelectronics BlueST SDK v2 as described below:

STMicroelectronics Manufacturer Advertising data
Byte Index 0 1 2-3 4 5 6 7 8 9 10-15
Function Length Manufacturer ID Company BlueST SDK Version Device ID Firmware ID Option 1 Option 2 Option 3 Device Address
Value 0x0F 0xFF 0x0030 STMicro 0x02 0x8B Nucleo-WBA 0xE2 - Connection subrating Server 0x00 0x00 0x00 0x08E12Axxxx


2.2. On-board buttons configuration

Button configuration for Bluetooth® Low Energy connection subrating application on Nucleo-WBA55CG boards
Application Condition B1 Click B1 Long Press B2 Click B2 Long Press B3 Click B3 Long Press
CS Server Idle

Connected

-

Starts/Stops notification

/ -

-

/ -

-

/
CS Client Idle

Connected

Starts scan then connects

Starts/Stops write data

/ -

-t

/ -

-

/

2.3. Database Hash characteristic

If the client and the server are not bonded, then the server assumes, that the client checks the Database Hash and/or discovers the GATT database upon each connection before initiating any GATT operation.

Bluetooth® Database Hash characteristic
connectivity database Hash charac5.png


2.4. Client Supported Features characteristic

If the client enables Robust Caching, by setting the Robust Caching bit to 1 in the Client Supported Features characteristic, then the server can send a database out-of-sync error code (0x12) as a response to a GATT operation whenever it assumes, that the client has an out-of-date database.

Bluetooth® Robust caching feature in Client Supported Features characteristic
connectivity robust caching ClientSupportedFeature charac7.png


If the client and the server are bonded, then the server checks if the database has changed since the last connection and notifies the client about the change via Service Change Indication - just like before introducing GATT caching.
The only difference is, that if the client initiates a GATT operation before the indication is received and confirmed, the server can send a database out-of-sync error code. This helps to avoid race condition if the client would like to initiate a GATT operation too quickly after connection establishment.

3. References

No categories assignedEdit