ImageMap

Revision as of 09:52, 18 October 2019 by wiki>Vincent Abriou (Created page with "<noinclude> ==Usage== The ImageMap template is used '''to enhance images with dynamic contents''' (explanations and links) using '''image maps''' (aka "c...")

1. Usage

The ImageMap template is used to enhance images with dynamic contents (explanations and links) using image maps (aka "clickable images"). An image map is a list of coordinates in an image, that links areas of the image to multiple destinations. In the STM32 MPU wiki, the image maps rely on:

Usage:  {{ImageMap | File:<filename>.<extension>{{!}}<options>{{!}}<caption>
        <list of coordinates> <list of explanations and links>
        }}

Where:

  • <filename>, <extension>, <options> and <caption> are defined in the images help page
  • <list of coordinates> are the coordinates of forms (rectangles, circles...) in the image
  • <list of explanations and links> are the explanations and links associated with these forms

2. Basic examples

Example of image map
You type
{{ImageMap|File: Image_map_example.png{{!}}thumb{{!}}center{{!}}Add your text legend here
rect 160 2 248 77 [[Contributors:Fake article | Step 1 (rectangle example)]]
poly 292 228 312 187 387 188 407 229 386 271 313 269 292 228 [[Contributors:Fake article | Step 2 (Polygon example)]]
circle 47 225 44 [[Contributors:Fake article | Step 3 (circle example)]]
poly 87 155 129 105 120 96 160 93 162 130 152 125 108 180 83 159 83 160 [[Contributors:Fake article | Arrows (multiple polygons example)]]
poly 137 225 162 199 163 212 253 212 252 243 163 242 163 253 137 225 [[Contributors:Fake article | Arrows (multiple polygons example)]]
poly 261 110 300 162 294 167 290 168 330 176 334 140 334 137 325 144 283 88 259 106 [[Contributors:Fake article | Arrows (multiple polygons example)]]
}}
You get
Step 1 (rectangle example)Step 2 (Polygon example)Step 3 (circle example)Arrows (multiple polygons example)Arrows (multiple polygons example)Arrows (multiple polygons example)
Add your text legend here
Info white.png Information
  • Areas which overlap give precedence to the first link listed: this gives the possibilities to create links on boxes that are drawn inside a bigger one, declaring the biggest box at the end of the list
  • Do not use <br>, but <br/> in image maps

3. References

4. Code

Error: Must specify an image in the first line.

No categories assignedEdit