This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The GDB$ template is used to prefix a command that must be executed on GDB, with a GDB-specific prompt.
Thanks to the gdb-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{GDB$}}
2. Basic examples
You type | You get |
---|---|
info break command executed on GDB
{{GDB$}} show listsize<br> Number of source lines gdb will list by default is 10. |
show listsize |
3. More examples
You type | You get |
---|---|
2 commands executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} show listsize Number of source lines gdb will list by default is 10. {{GDB$}} continue |
show listsize Number of source lines gdb will list by default is 10. continue |
Command executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} show listsize Number of source lines gdb will list by default is 10. |
show listsize Number of source lines gdb will list by default is 10. |
Long command executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} this is a so long command executed on GDB that a horizontal scrolling bar is needed |
this is a so long command executed on GDB that a horizontal scrolling bar is needed |
Template used within another public message box template
{{Info | Message before the command {{GDB$}} show listsize Number of source lines gdb will list by default is 10. Message after the command }} |
|
Template used within another protected message box template
{{InternalInfo | Message before the command {{GDB$}} show listsize Number of source lines gdb will list by default is 10. Message after the command }} |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code