How to install a trusted application on STM32N6 MCUs

Revision as of 17:12, 18 September 2024 by Registered User
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

How to install a trusted application on STM32N6 MCUs


Literature

  • UM2237 STM32CubeProgrammer software description
  • AN5054 Secure programming using STM32CubeProgrammer


Target description

  • How to sign / encrypt a basic application loaded by BootRom
  • Which OTPs are concerned by BootRom Authenticity and integrity checks
  • How to get the BootRom traces
  • How to set the device in closed-locked state


Introduction

Start by reading the Intro article.


Prerequisites

  • Hardware
    • STM32HN6 discovery board
    • Discovery MB1860- STM32N6 (need USBC cable)

thumb

  • Required tools
    • IAR : v9.40.1 + IAR patch to support STM32N6 (delivered with V0.5.0)
    • STM32CubeN6 FW version 0.5.0 & patch version 0.5.1 & 0.5.2
    • STM32CubeProgrammer version 0.0.2-N6-B03
    • Tera Term / Putty or equivalent terminal emulator
Info white.png Information
The TPC installed together with CubeProgrammer in the bin folder located in default STM32CubeProgrammer path : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin You can pin this tool to the taskbar to simplify the "STiRoT Getting started" process :
Security PinToTask.png


  • STM32Cube Firmware
    • Download the STM32Cube_FW_N6 Cube firmware (advise is to place it close form the C: in order to avoid long windows paths).
    • A directory STM32N6-DK is included in "STM32Cube_FW_N6\Projects" .


  • Open the env.bat file
  • 1- If the STM32CubeProgrammer has not been installed in the default folder:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer, the customized installation path needs to be updated.

  • 2- Update the COM port to be aligned with your COM port number.

Use the Windows device manager to find out your COM port number, as shown in figure below:

Security COM Port.png
  • 3- Check that the OEMiRoT_Appli path is OK. The picture below shows the configuration path for the STM32CubeFW example but it is possible to select an other application that respects OEMiRoT template.
SECURITY H7S OEMiRoT env bat 3.png
No categories assignedEdit